Article number | 6GK6015-0AL20-0GC1 | 6GK6015-0AL20-0GJ1 | |
product type designation | RX1500PN LM APE1402W7 | APE1808W10 | |
**** Replacement part **** RUGGEDCOM RX1500PN LM APE1402W7 Line Module Application Processing Engine 1.3Ghz, 2GB RAM, 8GB SSD, Windows 7 Embedded Conformal Coating | RUGGEDCOM APE1808W10 Application Processing Engine Line Module, Atom x5-E3940, 8GB RAM, 80GB eMMC, DisplayPort, uSD, USB, Windows 10 Conformal Coating | ||
hardware configuration | |||
design of the processor | Atom x5-E3940 | ||
processor clock frequency | 1.3 GHz | ||
design of the drive/storage medium / solid-state disk | Yes | Yes; eMMC | |
storage capacity / on solid-state disk | 64 Gibyte | ||
storage capacity / on hard disk | 8 Gibyte | ||
storage capacity / of the RAM | 2 Gibyte | 8 Gibyte | |
operating system / pre-installed | Windows Embedded 7 | Windows 10 | |
design, dimensions and weights | |||
product feature / conformal coating | Yes | Yes | |
further information / internet links | |||
internet link | |||
● to website: Selection guide for cables and connectors | https://siemens.com/tst | ||
● to website: Industrial communication | https://siemens.com/industrial-communication | ||
● to website: Image database | https://www.automation.siemens.com/bilddb | https://www.automation.siemens.com/bilddb | |
● to website: CAx-Download-Manager | https://siemens.com/cax | https://siemens.com/cax | |
● to website: Industry Online Support | https://support.industry.siemens.com | https://support.industry.siemens.com | |
security information | |||
security information | Siemens provides products and solutions with industrial cybersecurity functions that support the secure operation of plants, systems, machines and networks. In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial cybersecurity concept. Siemens’ products and solutions constitute one element of such a concept. Customers are responsible for preventing unauthorized access to their plants, systems, machines and networks. Such systems, machines and components should only be connected to an enterprise network or the internet if and to the extent such a connection is necessary and only when appropriate security measures (e.g. firewalls and/or network segmentation) are in place. For additional information on industrial cybersecurity measures that may be implemented, please visit www.siemens.com/cybersecurity-industry. Siemens’ products and solutions undergo continuous development to make them more secure. Siemens strongly recommends that product updates are applied as soon as they are available and that the latest product versions are used. Use of product versions that are no longer supported, and failure to apply the latest updates may increase customer’s exposure to cyber threats. To stay informed about product updates, subscribe to the Siemens Industrial Cybersecurity RSS Feed under https://www.siemens.com/cert. (V4.7) | Siemens provides products and solutions with industrial cybersecurity functions that support the secure operation of plants, systems, machines and networks. In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial cybersecurity concept. Siemens’ products and solutions constitute one element of such a concept. Customers are responsible for preventing unauthorized access to their plants, systems, machines and networks. Such systems, machines and components should only be connected to an enterprise network or the internet if and to the extent such a connection is necessary and only when appropriate security measures (e.g. firewalls and/or network segmentation) are in place. For additional information on industrial cybersecurity measures that may be implemented, please visit www.siemens.com/cybersecurity-industry. Siemens’ products and solutions undergo continuous development to make them more secure. Siemens strongly recommends that product updates are applied as soon as they are available and that the latest product versions are used. Use of product versions that are no longer supported, and failure to apply the latest updates may increase customer’s exposure to cyber threats. To stay informed about product updates, subscribe to the Siemens Industrial Cybersecurity RSS Feed under https://www.siemens.com/cert. (V4.7) | |
Approvals / Certificates | |||
General Product Approval | |||
Manufacturer Declaration | Yes | Yes | |
UK Declaration of Conformity | Yes | Yes | |
EU declaration of conformity | Yes | Yes | |
other | |||
inspection certificate | Yes | Yes | |
Dangerous Good | |||
Dangerous Goods Information | Yes | Yes | |
Environment | |||
EPD Typ II/III (with life cylce assessment) | Yes | Yes | |
last modified: | 3/25/2024 | ||
Date 5/2/2024 |
Subject to change without notice © Copyright Siemens 2024 |