SIRIUS ACT Configurator
News

By
means of the SIRUS ACT Configurator we provide a useful tool for you to fast
and easy configure customer specific products and order with the Industry Mall.
You have the choice to start the configurator between three entry
possibilities.
1.
Configuration of single
command points with actuators and signal devices on the front panel
Complete command points with different actuators, modules and
accessories (maximum of 24 command points) can be configured and labeled
customer-specific. In addition, key switches with special locks can be chosen.
2.
Configuration of customer
specific enclosures with command points
Here, you have opportunity of configuring the command points
of enclosures with various actuators, modules and accessories and also inscribe
the enclosure customer specific. Communication-capable variants (e. g.
AS-Interface) are also available.
3.
Configuration of single
components (e. g. actuating element, inscription plate etc.)
Through this selection you can configure single actuators/indicators,
empty enclosures, modules, accessories and holders. An extensive offer is
given. You also have the opportunity of labeling the single components
customer-specific.
Result area:
In the result area
technical and sales related data are supplied for your documentation. Furthermore,
list prices are displayed.
Order:
After completing the configuration, you can manually generate a CIN
(Configuration Identification Number). In case of a direct order via Mall-cart,
a CIN will be generated automatically. The configuration will be saved in our
system through the generated CIN. In addition to the Article No. the CIN must
be saved in your system and must be indicated as E-text in follow-up orders together
with the order code (KOY).
Example:
Information
dialog, automatically displayed after generating the CIN via the menu in the
configurator application.
![]()
Order
number: 3SU1801-0AZ00 K0Y = CIN20150609140858154554
The
ordering process is simplified by the use of the CIN-mechanism:
·
Configuration files don’t have to be saved by the user any
more
·
By means of CIN standard ordering ways can be used
·
Configuration files don’t have to be send to the plant via
email
We
will inform you about the latest activations of new functions and product
supplements via news area.
SIRIUS ACT - Team